cancel
Showing results for 
Search instead for 
Did you mean: 

Using TLC2543 ADC chip on STM32L476RG

paker earth
Associate II
Posted on February 08, 2017 at 11:33

Hi all

I followed the post below to setup tlc2543.

http://blog.csdn.net/haozi_1989/article/details/6111776

 

datasheet 

http://www.ti.com/lit/ds/symlink/tlc2543-ep.pdf

 

Because the STM32L4 series used HAL library not SPL, so I have to modify some codes.

But I still got random voltage values.

Could someone tell me if the modification is right, or how to solve it?

Thank you all in advance.

Here are related codes. SPI2 , PB1 use as CS

uint16_t Read_TLC2543(uint16_t chan)

{

   uint8_t data;

   uint16_t i,ADCdata;

   chan <<= 12;

   chan|= 0x0C00;

   //GPIO_WriteBit(GPIOA, GPIO_Pin_4, Bit_RESET);

   HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_RESET);

   for(i=0;i<2000;i++);//delay

   //while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)==RESET);

   while(((hspi2.Instance->SR) & SPI_FLAG_TXE) != SPI_FLAG_TXE) ;

   //SPI_I2S_SendData(SPI1,chan);

   if(HAL_SPI_Transmit(&hspi2, &chan, 2, 1000) != HAL_OK)

      printf('error1\r\n');

   //while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)==RESET) ;

   while(((hspi2.Instance->SR) & SPI_FLAG_RXNE) != SPI_FLAG_RXNE) ;

   //ADCdata=SPI_I2S_ReceiveData(SPI1);

   if(HAL_SPI_Receive(&hspi2, &ADCdata, 2, 1000) != HAL_OK)

      printf('error2\r\n');

   for(i=0;i<2000;i++);//delay

   ADCdata >>= 4;

   //GPIO_WriteBit(GPIOA, GPIO_Pin_4, Bit_SET);

   HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_SET);

   return ADCdata;

}

void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)

{

   GPIO_InitTypeDef GPIO_InitStruct;

   if(hspi->Instance==SPI2)

   {

   /* USER CODE BEGIN SPI2_MspInit 0 */

   /* USER CODE END SPI2_MspInit 0 */

   /* Peripheral clock enable */

   __HAL_RCC_SPI2_CLK_ENABLE();

   /**SPI2 GPIO Configuration

   PB13 ------> SPI2_SCK

   PB14 ------> SPI2_MISO

   PB15 ------> SPI2_MOSI

   */

   /* USER CODE BEGIN SPI2_MspInit 1 */

   /* Configure SPI SCK */

   GPIO_InitStruct.Pin = GPIO_PIN_13;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

   GPIO_InitStruct.Pull = GPIO_PULLUP;

   GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

   GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

   HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

   /* Configure SPI MISO and MOSI */

   GPIO_InitStruct.Pin = GPIO_PIN_15;

   GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

   GPIO_InitStruct.Pull = GPIO_PULLDOWN;

   HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

   GPIO_InitStruct.Pin = GPIO_PIN_14;

   HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

   /* USER CODE END SPI2_MspInit 1 */

   }

}

static void MX_SPI2_Init(void)

{

   hspi2.Instance = SPI2;

   hspi2.Init.Mode = SPI_MODE_MASTER;

   hspi2.Init.Direction = SPI_DIRECTION_2LINES;

   hspi2.Init.DataSize = SPI_DATASIZE_16BIT;

   hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;

   hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;

   hspi2.Init.NSS = SPI_NSS_SOFT;

   hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;

   hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;

   hspi2.Init.TIMode = SPI_TIMODE_DISABLE;

   hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;

   hspi2.Init.CRCPolynomial = 7;

   hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;

   hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;

   if (HAL_SPI_Init(&hspi2) != HAL_OK)

   {

      Error_Handler();

   }

}

#stm32l476rg
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on February 08, 2017 at 21:57

I would bit-bang the protocol first.

JW

T J
Lead
Posted on February 08, 2017 at 23:04

this is a very old chip, the data sheet is from 1993 !   thats 23 years old technology.

the conversion rate is 100KHz, good enough for most applications.

the price ?    $6 for 2000 pieces ???

that is crazy.

this chip has to be end of life soon. I would say, not recommended for new designs.

the data sheet shows that 16bit clocking is ok, so is this what you are doing ?

this line looks wrong:

 if(HAL_SPI_Transmit(&hspi2, &chan, 2, 1000) != HAL_OK)

after the initialisation :

   chan <<= 12;      

   chan|= 0x0C00;

&chan is the pointer to a data field with the transmission packet data

ie. chan[0] = FirstByte to be transmitted

ie. chan[1] = SecondByte to be transmitted

this looks like your problem...