cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5-UDESTK adapter voltage source

Andrew Tierney
Associate II
Posted on March 02, 2017 at 15:33

I have an SPC5-UDESTK JTAG adapter here, which I am using with UDE.

Does the adapter source it's own voltage, or do I need to feed voltage from the target back to it? If so, which pin is used?

Thanks

3 REPLIES 3
Erwan YVIN
ST Employee
Posted on March 03, 2017 at 11:11

Hello Andrew ,

Normally  , When plugged on the Board 

SPC5-UDESTK and USB Cable.

it should be ok.

the booard is supplying the voltage for SPC5-UDESTK

         Best regards

                           Erwan

Andrew Tierney
Associate II
Posted on March 03, 2017 at 14:57

So it seems that I need to provide voltage from the board back to the adapter on one of the pins. I seem to have found this pin as it makes one of the LEDs on the adapter light up.

Is there not any documentation about the pins and LEDs on the SPC5-UDESTK?

Is there anyway to chose internal voltage? 

Posted on March 09, 2017 at 11:06

Hello Andrew ,

Which board do you use ?

For a discovery Board, You do not need to use 

SPC5-UDESTK , the 

Discovery Board contains the hw debugger by FTDI (Usb), you have just to plug the mini usb cable.

            Best Regards

                               Erwan