Posted on March 02, 2017 at 16:52There don't seem to be any example projects or pin wizards for this board, although I can see it in some of the .c/.h files with the install. I have just updated SPC5-STUDIO so was expecting to see support.Are there ...
Posted on March 02, 2017 at 15:33I have an SPC5-UDESTK JTAG adapter here, which I am using with UDE.Does the adapter source it's own voltage, or do I need to feed voltage from the target back to it? If so, which pin is used?Thanks
Posted on March 02, 2017 at 14:27Hello,I am working with the SPC58EC80E1 and cannot find a datasheet for this product.Most urgently, I would like the pin out of the device in TQFP64.Can anyone point to where I could get this?Thanks,Andrew
Posted on March 03, 2017 at 14:57So it seems that I need to provide voltage from the board back to the adapter on one of the pins. I seem to have found this pin as it makes one of the LEDs on the adapter light up.Is there not any documentation about...