cancel
Showing results for 
Search instead for 
Did you mean: 

Question about SPWF01SA module

Alejandro Rivera
Associate
Posted on July 11, 2018 at 15:24

Hello,

I am using the SPWF01SA incorporated into a board with a microcontroller that is responsible for responding to orders that come through the module.

My problem is that through the page ''output_demo.html'' I can send messages without problem, but I have no option to view the messages I receive from the board. The ''input_demo.shtml'' page always shows me the following message:

0690X0000060M68QAE.png

Even if you check the first option always shows this. Is there any way to be able to visualize the messages that are sent from the board through this page?

Since I have this error, to see the messages sent from the board I open a socket with the command AT + SOCKD = 32000 and access it through the SocketTest program. So far everything is correct, but when I add the network to a local network with an internet connection, this socket disappears.

Is there any chance that when I add the network to another one, this socket it will remain open and I will be able to communicate through it?

Thanks

#spwf01sa #socket #wifi-sp*
0 REPLIES 0