Skip to main content
sirius506
Associate III
January 24, 2018
Question

STM32CubeProgrammer fails to connect to Nucleo-F767

Posted on January 24, 2018 at 10:26

I'd like to use STM32CubeProg with Nucleo-F767 via USB, but CubeProg fails to connect with 'Corrupted Data base' error. I've tried both Windows and MacOS versions, results same error.

I guess STM_Prog_DB.xml is the 'data base' file.  How can I fix this DB file?

Thanks in advance,

#stm32cubeprogrammer
This topic has been closed for replies.

3 replies

cazaux.clement
Visitor II
February 9, 2018
Posted on February 09, 2018 at 18:25

Hello,

I have the same issue while trying to use USB DFU on a board with STM32F779 NIH6 78A4U VQ Z:

0690X00000609enQAA.png

I do connect correctly with STLink connection:

0690X00000609cOQAQ.png

Does the issue come from my STM32 code or from the CubeProgrammer utility? What  is that ''Data base'' is '' Corrupted''?

Any help/clue would be appreciated!

Edit :

I also give a try with the command line utility, without success : (see capture below)

I think that the ''corrupted data base'' message that we get on CubeProgrammer GUI is due to the ''Device ID  Unknown''  where I could get '' DeviceID 0x451'' 

What is really puzzling is that Serial Number and firmware version is correctly read... Same behavior on the 10 boards that we produce.

0690X00000609hSQAQ.png
ST Technical Moderator
February 26, 2018
Posted on February 26, 2018 at 16:40

Hello,

This issue is already confirmed along to our development team and will be fixed in the coming release.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
cazaux.clement
Visitor II
February 26, 2018
Posted on February 26, 2018 at 17:03

Thank you for your reply Imen.

Can your tell us when this new release will come?

Best Regards,