cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-L152RET + STM32CubeProgrammer

Soham Jani
Associate II
Posted on March 02, 2018 at 21:49

I'm trying to use the dual bank feature in the Nucleo-l152re dev board. I want to understand how I can use program bank 2 (address 0x08040000) using the STM32Cube Programmer using the onboard USATR1.

I understand that I need to enter the boot mode using the BOOT0 pin, connect after system reset and flash by programming the appropriate image file. The problem is :

 -- I cannot find the option to choose the bank

-- the option to put in the start address is not highlighted. 

Although i can choose the value of option byte: checked for 0 or unchecked for 1, no point loading from bank 2 when there is nothing on there. 

Any help will be appreciated. 

#stm32cube-programmer #nucleo-l152re
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0