cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.23.0 syscalls.c bugs ?

Heiko Jakob
Associate
Posted on October 28, 2017 at 14:31

Hi,

i'm using STM32CubeMX V 4.23.0 to build a project for a stm32f107vct with FatFs, LWIP & FreeRTOS using the gcc-arm-none-eabi-6-2017-q2-update toolchain.

Compiling the generated syscalls.c fails due various errors (see output below).

  1. One problem is that '

    #

    ifdef

    _SYS_TIME_H_' should be '

    #

    ifndef

    _SYS_TIME_H_', because timezone is already defined via the generated <sys/time.h> include in gcc-arm-none-eabi-6-2017-q2-update/arm-none-eabi/include/sys/time.h and _SYS_TIME_H_ is therefore already set.

    #ifdef _SYS_TIME_H_

    struct timezone {

    int tz_minuteswest; /* minutes west of Greenwich */

    int tz_dsttime; /* type of dst correction */

    };

    #endif

  2. gcc relies on __asm_() instead asm() when using ANSI-C or STD-C so the following generated statement should be changed

    caddr_t _sbrk(int incr)

    {

    extern char end

    asm

    ('end'); // should be

    __

    asm__

    ('end');

    static char *heap_end;

    char *prev_heap_end,*min_stack_ptr;

With best regards

Heiko Jakob

arm-none-eabi-gcc -mthumb -mcpu=cortex-m3 -mfloat-abi=soft -ffunction-sections -fdata-sections -Os -flto -fno-exceptions -Wall -DSTM32F107xC -c -g -Iinclude -Ilib/STM32CubeMX/Inc -Ilib/STM32CubeMX/Drivers/CMSIS/Include -Ilib/STM32CubeMX/Drivers/STM32F1xx_HAL_Driver/Inc -Ilib/STM32CubeMX/Drivers/CMSIS/Device/ST/STM32F1xx/Include -Ilib/STM32CubeMX/Middlewares/Third_Party/LwIP/src/include -Ilib/STM32CubeMX/Middlewares/Third_Party/LwIP/system -Ilib/STM32CubeMX/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -Ilib/STM32CubeMX/Middlewares/Third_Party/FreeRTOS/Source/include -Ilib/STM32CubeMX/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM3 -Ilib/STM32CubeMX/Middlewares/Third_Party/FatFs/src -Ilib/STM32CubeMX/Middlewares/ST/STM32_USB_Device_Library/Core/Inc -std=c11 -MMD -MP -MF 'build/Debug/GNU_ARM_NONE_EABI_6_2017Q2-Linux/lib/STM32CubeMX/Src/syscalls.o.d' -o build/Debug/GNU_ARM_NONE_EABI_6_2017Q2-Linux/lib/STM32CubeMX/Src/syscalls.o lib/STM32CubeMX/Src/syscalls.c

lib/STM32CubeMX/Src/syscalls.c: In function '_sbrk':

lib/STM32CubeMX/Src/syscalls.c:98:18: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'asm'

extern char end asm('end');

^~~

lib/STM32CubeMX/Src/syscalls.c:98:18: warning: implicit declaration of function 'asm' [-Wimplicit-function-declaration]

lib/STM32CubeMX/Src/syscalls.c:103:15: error: 'end' undeclared (first use in this function)

heap_end = &end;

^~~

lib/STM32CubeMX/Src/syscalls.c:103:15: note: each undeclared identifier is reported only once for each function it appears in

lib/STM32CubeMX/Src/syscalls.c: At top level:

lib/STM32CubeMX/Src/syscalls.c:129:8: error: redefinition of 'struct timezone'

struct timezone {

^~~~~~~~

In file included from lib/STM32CubeMX/Src/syscalls.c:75:0:

/opt/gcc-arm-none-eabi-6-2017-q2-update/arm-none-eabi/include/sys/time.h:50:8: note: originally defined here

struct timezone {

^~~~~~~~
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee
Posted on October 30, 2017 at 11:49

Hello

jakob.heiko

,

I confirm your reported issue and I raised it internally to the appropriate team.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Sirma Siang
ST Employee
Posted on October 30, 2017 at 16:59

Hello

jakob.heiko

,

I first thank you for your comment.

The timezone definition was necessary because of lwip:sockets.h. That code is coming from LWIP community and ST does not change it.

To avoid the timeval multidefinition, the pragma_SYS_TIME_H_ had to be defined at build level (btw: you should have it in the generated makefile), thus timezone had to be added 'manually', and this is done in the syscalls.c.

Have you modified the generated makefile ?

Kind regards

Sirma

Cyril FENARD
ST Employee
Posted on May 04, 2018 at 13:45

Hi

jakob.heiko

‌,

Most recent available version of CubeMX I used, i.e. 4.25, brings new defines for compilation line in Makefile.

Please find here after some evidence log:

make -C Canada_MkI BINPATH=/cygdrive/c/gcc-arm/bin -f Makefile -k

make: Entering directory '/cygdrive/i/STM32/CUBE_MX/CubeMX_7921/support/Canada_MkI'

mkdir build

...

/cygdrive/c/gcc-arm/bin/arm-none-eabi-gcc -c -mcpu=cortex-m3 -mthumb -D_TIMEVAL_DEFINED -D_SYS_TIME_H_ -DUSE_HAL_DRIVER -DSTM32F107xC -DUSE_FULL_LL_DRIVER

-I../Inc

...

-Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF'build/ethip6.d' -MT'build/ethip6.d'

-Wa,-a,-ad,-alms=build/ethip6.lst ../Middlewares/Third_Party/LwIP/src/core/ipv6/ethip6.c -o build/ethip6.o

...

/cygdrive/c/gcc-arm/bin/arm-none-eabi-size build/Canada_MkI.elf

text data bss dec hex filename

86072 500 41364 127936 1f3c0 build/Canada_MkI.elf

/cygdrive/c/gcc-arm/bin/arm-none-eabi-objcopy -O ihex build/Canada_MkI.elf build/Canada_MkI.hex

/cygdrive/c/gcc-arm/bin/arm-none-eabi-objcopy -O binary -S build/Canada_MkI.elf build/Canada_MkI.bin

make: Leaving directory '/cygdrive/i/STM32/CUBE_MX/CubeMX_7921/support/Canada_MkI'

NOTE: I modified the 'Project Settings', i.e.,in 'Advance Settings', 'Driver Selector' as LL for RTC.

Hope this helps completing this thread.

Regards.

Cyril