Posted on October 17, 2017 at 18:03 I tested three devices all day long today. All devices are connected to the USART, but the incoming interrupt does not work at all. A program that connects the Lo Ra modules, GPS modules, and wifi mod...
Posted on October 05, 2017 at 07:58I am under test for I2C. Setting of CubeMX does not allow the pullup/down setting. The I2C device used is htu-21d (Humidity and Humidity Sensor).--source code--.. i2cTxData = (uint8_t)0xe3; // temp while(HAL_I2C...
Posted on March 14, 2017 at 08:18I think the new issue seems to have a problem with source generation.When choosing the HSE, create the source as follows : RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;To operate ...
Posted on January 29, 2017 at 17:22The attached project is made up of CubeMX 4.18.0.If you open the project after opening the project at CubeMX 4.19.0 and then creating source again, an error occurs.
Posted on January 12, 2017 at 08:34hiI'm using CubeMX 4.18.0 recently.by the way, Every time An error occurs when creating a TrueStudio project using the CubeMX 4.18.0.Please, help.#cubemx #truestudio
Posted on October 21, 2017 at 06:19At 9600 bps, sometimes rx interrupt stops. Sometimes it stops in a few minutes or stops in a matter of hours.However, the scope can still confirm that the data is still transferred.The problem remains unsolved.
Posted on October 21, 2017 at 06:13At 9600 bps, sometimes rx interrupt stops.Sometimes it stops in a few minutes or stops in a matter of hours.However, the scope can still confirm that the data is still transferred.The problem remains unsolved.
Posted on October 20, 2017 at 03:37HiI tested it all day long.test result is 1.If the device and the baud rate are between 115200bps, DO NOT enter the Rx Interrupt.2. If i have 9600bps the speed between devices and boards, enter the Rx Interrupt poi...
Posted on October 20, 2017 at 02:24 hi This is the ADC sample code for stm32f103c8t6 that I made. I attach my own code because I am not competent to advise you.
________________
Attachments : STM32ADC.zip : https://st--c.eu10.content.force.com...