cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.19.0 Problem report.

SoHaeng.Lee
Associate II
Posted on January 29, 2017 at 17:22

The attached project is made up of CubeMX 4.18.0.

If you open the project after opening the project at CubeMX 4.19.0 and then creating source again, an error occurs.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
stm32cube-t
ST Employee
Posted on February 01, 2017 at 12:21

Hello,

This is a known issue with MX 4.18.

Please use the import feature in MX 4.19:

Start by creating a new project, selecting the STM32F103C8Tx MCU  (as used in your 4.18 project),

then select the menu File > import to import your 4.18 ioc file.

You will need to redo the clock tree configuration that could not be automatically imported.

But, project generation will work fine then.

View solution in original post

2 REPLIES 2
Imen.D
ST Employee
Posted on January 29, 2017 at 21:46

Hi

SoHaeng.Lee

‌,

I will check this issue and come back to you as soon as possible.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
stm32cube-t
ST Employee
Posted on February 01, 2017 at 12:21

Hello,

This is a known issue with MX 4.18.

Please use the import feature in MX 4.19:

Start by creating a new project, selecting the STM32F103C8Tx MCU  (as used in your 4.18 project),

then select the menu File > import to import your 4.18 ioc file.

You will need to redo the clock tree configuration that could not be automatically imported.

But, project generation will work fine then.