Hi,The evaluation GUI V2.8 should work with L9963E boards with Firmware 1.6 and above. For L9963 boards with firmware 1.5 , evaluation GUI V1.8 and below should be used. In any case, after clearing the IDs, please only click Configure ID ONCE. After ...
Hi,From your picture, you are missing 1 jumper for JHOT. Connect pins 1-2 for JHOT.You need to power up the L9963E ( in your case , the 20V DC ) , then power up the 12V DC for the MCU. So after power down, power up L9963E, then power up 12V for MCU. ...
Hi,Please try attached script. You need to go to Register Load , and open the file from there. After that, the script will be selectable in "Script Select".The L9961 board needs to be power by 12V DC at B+ / B- . In the manual, the STM32 nucleo board...
Hi,It is in the latest datasheet dated 18th Jan 2023 - https://www.st.com/en/power-management/l9961.html#documentation DS14012Battery management system solution v 3.0 Open in Adobe Reader, click on attachments on the left, it is an excel file