Hello @pjrebordao,regarding the ESC timer configuration, the Timer is not configurable and set by default to TImer2Besides, into a G431B-ESC1 project, Timer1 is set by default (and not configurable) for phases control with PWM signals. Only the Speed...
Hello @pjrebordao,First if not already read, i advise you to have a look to the following document:UM2516Electronic speed controller Discovery kit for drones with STM32G431CBBy reading the chapter 6, you will be able to control the speed of the motor...
Hi Prasanth91, 1. I invite you to download the last version of the STM32 MCSDK 6.3.1 package.MCSDK 6.3.1 is out ! - STMicroelectronics CommunityInto the Motor Control Workbench tool, you will find an example project (6-Step example on IHM03 pack and ...
Hi Sayali, this Open-Loop + Hall sensored project is now supported.For that purpose, i invite you to download the new version of the MCSDK 6.3.1.https://community.st.com/t5/stm32-mcus-motor-control/mcsdk-6-3-1-is-out/td-p/723764 Best regards.Fabrice
Hi arpituee, there are two ideas that could help.1. Depending on the 6-step driving mode you configured with the MCSDK6.3.0 workbench, you need to set up a specific jumper JP8 on the board as described into the user manual UMM2278 STEVAL-SPIN3202 - S...