Hi arpituee, there are two ideas that could help.1. Depending on the 6-step driving mode you configured with the MCSDK6.3.0 workbench, you need to set up a specific jumper JP8 on the board as described into the user manual UMM2278 STEVAL-SPIN3202 - S...
Hi GustavEckerbom,i do not see any reason why the STM F0/C0 family does not support your project as STM G4/F4 one does. Differences are mainly linked to the 16bits/32 bits computation and the ADC/timer IPs usages. As 6-step algorithm does not requi...
Hi Gary,Yes, we invite you to remove these capacitors on the power boards. The resulting RC time constant is not adapted to the PWM frequencies we are using for the motor control algorithms. Secondly, yes use the MCSDK6.3.0 that supersedes the STSW-S...
Hi murpia, these two examples STEVAL-PTOOL1V1_6S_HL.ioc and STEVAL-PTOOL1V1_6S_SL.ioc must be generated with the followed setup (information embedded into the IOC file):STM32Cube FW_F0 V1.11.4CubeMxCube.Version=6.9.1 or above (i used 6.9.11)MCSDK_v6....
Hi Gary_Baldy,the Motor Profiler SW is based on a FOC algorithm, then you need to generate a FOC project with the feature Motor Profiler enabled in Application Configuration as you mentioned and profile your motor with this SW.Load this SW into the b...