User Activity

Hello, I am using STM32U5G9ZJTxQ-DK2. I was wondering if the FiFo option from the UART can replace a ring buffer implementation ? I couldn't find much information on the UART FIFO, most documentations and examples are referring to DMA FIFO used with ...
Hello,I only have 2 GPIOs activated, and the SMPS, not yet any code written from me...The function HAL_PWREx_ControlVoltageScaling times out in NonSecure (somehow works if debugging and stepping into.. but then HAL_RCC_OscConfig get HAL_Error).For so...
Hello, I am trying to receive and transmit byte-to-byte on a STM32F429 Discovery, I will be using a STM32U5 Discovery soon. I used UART IT method but maybe there is a better solution...Objective & Issue:I want to continuously receive and send byte-to...
Kudos given to