User Activity

Hi I am working with the STM32MP257FxEV1 and trying to create a bare metal test project for evaluating the M33, since there is no ready example that can be created from the STM32Cube IDE I succeeded to create the project and build it correctly, also ...
Hello  Continue to me development on the STM32MP257xEV1, previous failure with the Python crypto packages  the project: OpenAMP_TTY_echo is loaded correctly, built configuration _ns_sign is completed OK, also looks like the .bin file is generated    ...
Hello  I'm starting development on the STM32MP257xEV1 (I already have an experience with the STM32CubeIDE with lots of MCUs) I followed the installation instructions, IDE 1.17 => and the MP2 package + patch => Python packages  I'm running on windows ...