After I installed the CubeIDE (STM32CubeIDE-Mac) on my mac with the delivered iinstaller, I cannot find the CubeIDE what is the name of the application? in which folder it is installed?
The Solution to this was the the PKG Archive consists of two things - an installer for a server application which I executed and an application file wich has to be copied into te application folder. this file was hides by the lower border of the wind...