User Activity

I am working on a project to connect QSPI flash memory to a PC as a USB mass storage device (MSC) using USBX, FILEX, LVLX, and THREADX on an STM32. This setup should allow the QSPI flash to appear as a drive in Windows.Previously, I successfully impl...
I am trying to make a custom external loader for a qspi nor flash. the erase sector and write operation is success but after I tried the read operation the operation is fail the device is disconnected and showing this message I have tried to run a pr...
I have designed a custom board using STM32H573IIT3Q MCU. when I connected it with st link, the st link not recognize it. After I check the voltage on power pin, all the power pin is normal except the VCAP pin (not outputing voltage). According to the...
Kudos given to