Thanks for a very swift and accurate reply Alessio!Activating the "POTENTIOMETER" flag made CubeMX add that pin, but nothing shows up in the code as far as I can see. What is the intended function of this flag in the code (and behavour when running t...
Hi ADAVE.1 or other ST EmployeesI just started to use EVLDRIVE101-HPD for a 36V 50W hallsensor PMSM motor. The SW creation process (MotorControllerWorkBench -> STMCubeMx -> STMCubeIDE -> Build Project) works fine and I can build and debug the code. H...