User Activity

I conducted an experiment with the following settings and results: LTDC - 0x20020000 (Internal RAM), Display - 0x20020000 (SDRAM): Display output is visible.LTDC - 0xC0000000 (SDRAM), Display - 0xC0000000 (SDRAM): No display output.LTDC - 0xC0000000 ...
Hello,I recently created a custom board using the STM32F746. I'm encountering an issue with the QSPI interface. The problem arose when I replaced the external flash from the MT25QL128ABA model to the IS25LP128F model. I have checked the data sheet an...
Hello, I'm developing using stm32f476-DISCO. Until now, we have made development easy by using external RAM. The current operation has received a request to create a program using only internal RAM without external RAM.   https://support.touchgfx.com...