User Activity

Hi ST Community, I’m working on a hardware design using the STM32H7A3 in an LQFP64 package, specifically STM32H7A3RIT and need some reassurance on the power supply configuration. I’ve been looking into the power domains outlined in the application no...
Hello there,I've encountered a problem when running motors with the F0 and C0 families. Perhaps this is already a known limitation, but I thought it still deserves a post.I don't need this to be solved, as I won’t be using these controllers for my pa...
Hi there,I'm writing this post because I have encountered a potential bug/firmware issue with the MC firmware versions FW1.11.4/FW1.11.5 for the F0 fam, and I'm unsure on how to proceed in diagnosing the cause of this problem.Background:I want to use...
Hello! I'm trying to configure the following setup to run the motor profiler in order to characterize a set of small/low-power BLDC motors. Configuration:I'm using MCWB 6.21Control board: Nucleo F401RE in the following configuration:JP5 at U5V,JP1 OF...