Hello, You're right there is no source file in the directory, however there is a readme.txt filec:\STM32_packages\STM32Cube_FW_WB_V1.19.0\Projects\STM32WB5MM-DK\Applications\Demontrations\Audio_BVLINKWB\readme.txtIt contains a link to the demonstrati...
Hello,Just in case, to measure current consumption you must not be in debug mode.You must flash the board then unplug and plug the power supply then measure the current.Regards,
Hello Chani,How to add FreeRTOS support to Azure RTOS packageThe main idea is to download an add-on and to apply it over XCC (based on Azure RTOS).It adds all the required files to get Cellular using FreeRTOS / LwIP up & running.Both X-CUBE-CELLULAR,...
Do not "trace off"And:at at%getacfg=radiom.config.preferred_rat_listYour trace indicates : at at%setacfg=radiom.config.preferred_rat_list,CAT"CATM"which is noit the command I provide you.Thank you