HI, STM Experts, Using STM32CubeIDE, I configured a project with default settings for the STM32H563ZIT6 (8 MHz external clock), running at 250 MHz. Additionally, I've enabled SPI1 for full duplex communication (transmitting and receivi...
Hi, I would like to check whether it is possible to perform internal SPI full duplex loop back tests on the STM32H563ZIT6 board, but I don't know how to do it.any one please help me.
Hi,I'm trying to interface audio output to the STM32H563ZIT6 microcontroller. I want to use GPDMA1 with the DAC, but I don't know how to configured GPDMA1 on STM32 CUBE IDE. Can anyone help me, please?
HI,i am trying to interface the HX711 Load Cell to STM32G0B1RCT6 Microcontroller.i using internal clock source(HCLK = 16MHz) and its reading good.Load Cell Value: 8220309Load Cell Value: 8221048Load Cell Value: 8221228Load Cell Value: 8221368Load Ce...
Hi, I am using the STM32H563ZIT6 microcontroller and trying to interface it with an internal DAC to a speaker through an external MCP601 op-amp. I am generating a sine wave on that DAC pin, but it is producing some noise in the speaker. I am unsure h...
Hi, @AScha.3. Actually, I want 65K colors (16-bit data, R: 5-bit, G: 6-bit, B: 5-bit), so I set the value of EPF [1:0] to 00. Is this the correct value for 16-bit color? i am little stuck..
@AScha.3 I checked that the SPI is working well on the oscilloscope and i saw the signal also, but the TFT is still not working. i want small changes in my TFT like showing bg color.if i get anything,easily i will take into another level.