Is there an application or example about an "audio playback" project using the SAI interface (SAIA-SAIB) connected to a Codec ?I'm using the Nucleo NUH723ZG board. Thank you, Carlo
I'm using the NUCLEO board NUH723 to develop a project and I need to understand better how the HAL_SAI_Transmit_IT works.
In my code I use the HAL_SAI_Transmit_IT to send data to the SAI1 interface --> 48KHz, stereo,32bit:
I have to send two buffer o...
Hi,I'm using a NUCLEO-H723ZG and I've installed the CMSIS DSP library, but when I try to compile the code something goes wrong... May you help me to understand what do I make wrong ? Thank you, Luigi
Hi,I need to use the I2S (or SAI) interface to connect a codec stereo working at 48KHz, 32bit word length and I2S connection; when I configure the multimedia I can select the SAI interface (SAI1 or SAI4) or one of the I2S interface available.Which ar...
Thank you,I've bought the V3, I'm using the STM32H723 (I'm not still decided if 144 or 100 pins) to develop a new project; is there a schematic that shows the jtag connector (and connections) needed for a project board ? Luigi