User Activity

hello forumI'm trying to make a new project from base stuff on both the BSP and JPEG_EncodingUsingFs_DMA examplesI have been trying to follow the How to add a BSP to an STM32CubeIDE project.  manual to the letter but, even after making sure all the p...
hello forumI've been playing with a H747I-Discovery board, and I want to add some more functionality to a combination of example codes - activating one of the i2c.the example itself doesn't include an .IOC file.As I see it I have two options:1.Start ...
hello forumI'm trying to use two examples at once, I'm looking for a script to save an image on an SD card as Jpegthe examples are:BSPJPEG_EncodingUsingFs_DMAI'm trying to import the JPEG_Encoding example into the BSP one,While doing so, the compiler...
Hello forum,I'm trying to use the BSP driver while implementing a USB Host functionality. after the initiation of everything the USB needs, the BSP started to raise a lot of errors of undeclared/undefined stuff, after checking I saw that the error wa...
Hello forum,Im trying to create a code for reading from and writing to a USB flash drive using the USB-C connector,While activating the USBPD, USBX, TCPP, and FileX, the code generated missing some defines and variables like "DPM_Ports", "PWR_Port_PD...
Kudos from