User Activity

I am trying to get data from ASM330LLHXG1 so first, I decided to try the self test code provided by ST to see whether I can make the sensor work, until the reading of status register it was going okay but no matter how long I wait the status register...
Hello everyone,I am currently developing an IMU array application using the ASM330LHHXG1 sensor and am trying to streamline my interrupt management. This sensor has two interrupt pins, and I am contemplating whether to use both pins or just one. My p...
Hello everyone,I'm working on a project using STM32 and I'm facing a recurring issue with the STM32CubeIDE and the HAL library concerning the SPI_DMATransmitReceiveCplt() function It is a static function so rewriting it in another source causes error...
Hi everyone,I'm facing an issue with using DMA1 for SPI communication in my project. I'm trying to achieve a 2 kHz frequency, but DMA1 doesn't seem to work at this rate, whereas BDMA functions without any problems. This is my sampling task that is ca...
 Hello,I have been working on creating an SPI loop using the SPI callback function to alternate between two sensors that share a common SPI SDI/SDO line. However, I am encountering an issue where the SPI transfer complete callback is triggered, but t...
Kudos from