User Activity

I am developing a device that implements the USB device class.According to application note AN4879 "Introduction to USB Hardware and PCB Design Considerations Using STM32 Microcontrollers" it is written as follows:Based on the USB specification, a US...
Hello.I am using mb1191-F746NGH6-C01, IAR Embedded Workbench for ARM 9.50.1.69506, CubeMX V6.12.1 andTouchGFX V6.22.0. I generated the project in TouchGFX for IAR. TouchGFX locate the backgrounds and widgets in external flash memory. The Discovery ST...
Hi, I am using STM32F746G_DISCO, STM32 CubeMX version: 6.11.1, STM32CubeIDE version: 1.15.0 and FW_F7 firmware package V1.17.1.I tested the project: \STM32F746GDISCOVERY\STM32Cube_FW_F7_V1.17.0\Projects\STM32746G-Discovery\Applications\USB_Device\MSC...