2015-11-17 6:05 AM
Between the rev 4 & Rev 6 datasheets there seems to have been a change in the centre pad size on the recommended footprint. It now seems to ask for 8mm max x6mm max - previously it was specified as 10mmx8mm! I have based all my designs on the larger pad.
The datasheet revision history does not seem to mention this change. When did it come in? Has there been a revison change on the module? #spwf01sa2015-11-17 6:43 AM
Hi Toby,
changes took place in Rev5.Module's HW did not change. I mean, there was only a mismatch on picture number 7. Pad size was (and is still) 8x6mm.Normally solder paste takes 80% of pad layout. You can reduce this percentage to 60%.Regardsjerry2015-11-17 6:53 AM
Ok thanks for the info. I will have to update my footprint to match for the next production boards.
Unfortunately then I assume that then there is potentially a risk of shorts then with the larger pad and our current production assemblies?2015-11-17 7:03 AM
Within 60% there are no risks, because of solder resist (vias are ok)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.