User Activity

Hi, I am using STM32F767ZI for ethernet communication. I update my CUBEIDE version from 1.16.1 to 1.17 latest version. After I update my ethernet program was show HardFault_Handler() during Execution. This was working fine in the previous version(1.1...
Hi Team, I am Using NUCLEO-F767ZI board for Ethernet interface. After all Ethernet configuration. The code shows lots of error which is attached below. Guide me how to rectify this error, what mistake I was done during configuration and programming.T...
Hello,I am using the STM32H743ZI Nucleo board.Suddenly The Red LED (Over current LED) is glowing in my Microcontroller. I have checked all the connections properly, and there is no short circuit.Because of this I can't able to load the Program in it ...
Hi team, I am doing experiment with NUCLEO-F439ZI board. after some time the LD4 "LED" was not glow. after I unplug the USB cable and reconnect the windows shows the flowing  error"Power surge on the USB port – Unknown USB Device needs more power tha...
Hi team,I have rotary encoder (Model - OVW2 -2048-2MC). Its resolution is 2048P/R. I get the encoder count via uart, but I have a problem, when encoder rotate continuously it does not give the data via uart, move slowly the encoder it update the valu...