Hello @imikec, There is already a request to add Docker support for STM32TrustedPackageCreator_CLI.Internal ticket number: 185103 (This is an internal tracking number and is not accessible or usable by customers).If you need any further assistance wi...
Hello @zax After investigation, the Errors when trying to flash the image are normal behavior since you are trying to use almost all of the memory, and in STM32WB5 not all the flash memory is accessible by the user, it contains both User application ...
Hello @zax,Regarding the programming Issue, it appears to be related to sectors when flashing large images. I have raised this issue internally for resolution.Internal ticket number: 193831 (This is an internal tracking number and is not accessible o...
Hello @RyanSkyports,The OpenSSL version you mentioned is the one used in the updater.Currently CubeProgrammer v2.16 and v2.17 both use OpenSSL v1.1.1:c:\program files\stmicroelectronics\stm32cube\stm32cubeprogrammer\bin\libcrypto-1_1-x64.dllThere is ...