User Activity

Hi,We are developing a LoRa application using the STM32WLE5JC chip. The product is to be implemented for multiple deployment regions (EU, US, AU and AS). We have a problem with the US configuration. When a device sends a join request, the first attem...
Hi,I'm working with the STM32WLE5JC mcu and Cube firmware 1.13.0. Can someone explain how the module/stack implements adaptive data rate? I can see from lora_app.h that it is enabled by default, but exactly how is it implemented?The screenshot is fro...
HelloWe are working on a product using the STM32WLE5JC MCU. The features a magnetic switch that generates interrupts (specifically a low to high transition) which is meant to wake up the MCU from STOP2 mode. What is the ideal way to do this? We have ...
We're using the STM32WLE5JC to develop a LoRa-based project. We are looking into testing our sensor in a very specific environment with very specific settings - the TX power and Spreading Factor. Can these two be manually configured?Thanks
Hello, I am working on a project using the STM32WLE5JC module and STM32CubeIDE for development, with firmware packge v.1.3.0.We are currently running EMC tests at a test facility, and they have requested for the ability for the device to send data ev...
Kudos from
Kudos given to