Well that will be an improvement. But you could make our lives easier if you just got rid of this need to log-in. If you need to provide instructions on how to set up a network connection then you are making things more complicated than they need to ...
I'm also finding this problem. I suspect the HAL lib code doesn't take the TIMPRE setting into account and thus it calculates the wrong divider settings for the timer.
HelloI have the same problem mentioned in the original post. I'm generating code for a NUCLEO-F429ZI board with the CubeIDE version 1.14.1. I've selected TIM6 for the timebase and I also see a tick every 0.5ms (should be 1ms).In HAL_TIM_PeriodElapsed...
The log-in function in my IDE isn't even working. It just does nothing.So now I'm stuck.ST... we really don't need this log-in nonsense.If you really must force it on us, you need to make sure it is 100% reliable - and it ain't.This is wasting my v...