AlwaysFlyingMon
key
Associate
since
2024-02-29
2024-05-23
User statistics
3
Posts
0
Solutions
1
Kudos given
1
Kudos received
View all badges
STMicroelectronics Community
About AlwaysFlyingMonkey
Options
Report User
User Activity
Posts
Replies
STM32U575 ADC1 AWD1 Interrupt handler abnormal
2024-05-23
The awd1 interrupt is enabled. The flags of awd1 and EOS are set before entering the ADC1_IRQHandler. If the flag of awd1 is handled first in the ADC1_IRQHandler, the flag of EOS will not be handled. If the flag of EOS is handled first in th...
LPDMA Update Link Error
2024-02-29
static uint16_t aDST_Buffer_1[BUFFER_SIZE] = {0}; static uint16_t aDST_Buffer_2[BUFFER_SIZE] = {0}; LL_DMA_LinkNodeTypeDef pNode1, pNode2; /** * @brief LPDMA1 transfer configuration * @PAram None * @retval None */ void BspLPDMA1Init(void) { /*...
Re: LPDMA Update Link Error
2024-02-29
__attribute__((section(".sram4"))) static uint16_t aDST_Buffer_1[BUFFER_SIZE] = {0};__attribute__((section(".sram4"))) static uint16_t aDST_Buffer_2[BUFFER_SIZE] = {0};__attribute__((section(".sram4"))) LL_DMA_LinkNodeTypeDef pNode1, pNode2; I solve ...
Kudos from
User
Count
Sarra.S
1
View all
Kudos given to
User
Count
Sarra.S
1
View all