User Activity

I'm trying to experiment with a Custom HID USB demo.I'm following the instructions at:How to implement a USB device custom HID class on ... - STMicroelectronics CommunityPart way down it suggests:However when I got to Middleware I don't have USB_DEVI...
I'm using at STM32H563VITz in LQFP100 package.According to the reference manual (RM0481 Rev 21209) I can use the internal Voltage Reference (and then set it to 2.0478V)I've also referenced the post at: How to configure VREFBUF on my STM32 - STMicroel...
I'm using a NUCLEO-H563ZI and the STM32 HAL (generated by CubeMX) and there's no data (and no activity) on any of the SPI lines.I'm using SPI2 and it is configured as follows:   static void MX_SPI2_Init(void) { /* USER CODE BEGIN SPI2_Init 0 */ ...
I have a brand new, out-of-the-box (i.e. I've not moved any of the jumpers) STM32H573I Dev Kit, When I plug in a USB-C cable into the CN10 port. Windows 10 informs me that the "USB device is not recognised".I've tried installing the ST-Link USB Drive...
Kudos from
Kudos given to