User Activity

I have a STM32F411 board connected with a GPS module connected onto USART2I also have Tim1 and Tim3 configured for PWM generation on their channels respectively.I am running a list of commands (from an array) to execute line for line.Most of the exec...
While testing the Blackpill Timers and Usarts I came across this problem. If I set for example 6 timer channels using two timers. (In my case Tim2 and Tim3 and Usart1. If I set all six channels to PWM generation, I find it difficult to dynamically re...
I need to download and populate the STM32 board selector. Currently in order to select a board, eg: Nucleo series, I will need an internet connection. Is there not a way to download the list and use STM32Cube IDE to select from the downloaded list? T...
STMCubeIDE seems to give endless problems. Since the MX can generate c++ code what is the possibility of using all the generated files in C++ Builder? If This is possible, which files should I look for? Has anyone tried this before or will we just ha...
HelloI tried everything but I cannot get STM32CubeIDE to get the editor to work.I just keep on getting this message: There is no active editor that provides an outline.I spent hours re-installing but nothing workedAll help will be appreciated
Kudos from