Skip to main content
Associate II
February 2, 2024
Solved

SIL 2/SIL 3 Microcontroller requirement

  • February 2, 2024
  • 2 replies
  • 2869 views

hi

we have requirement of SIL2/ SIL3 verified microcontroller which have 24 adc channel, UART(2), ETHERNET, CAN(2),SPI,I2C, 512KB FLASH ETC.

kindly suggest us

 

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
February 2, 2024
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
February 2, 2024

https://www.st.com/content/st_com/en/ecosystems/functionalsafety.html

 

Also note that SIL2/3 is a requirement on the system, not a microcontroller. There are no verified SIL2/3 microcontrollers. But many STM32 chips can be part of a system that is SIL2/3 verified if programmed correctly.

"If you feel a post has answered your question, please click ""Accept as Solution""."