User Activity

The FLASH has (what will become) a bootloader, and an application.I can successfully jump from bootloader to application without issue.The application communicates over USART, through a CP210x components, to a USB-A connector, and to an Android appli...
I am working with an STM32F107VCT6TR MCU to communicate with an M95M04-DRMN6TP component over SPI3.The pins are set up as follows:PB7(93) -> HOLD(7)PB6(92) -> W(3)PA15(77) -> S(1)PB5(91) SPI3_MOSI -> D(5)PB4(90) SPI3_MISO -> Q(2)PB3(89) SPI3_SCK -> C...
I am not a hardware tech, but am familiar with some bit-fiddly work in software.  Still, I am new to modern firmware development, and could likely use a pointing finger.I've been tasked to write firmware with these two components.The board is built, ...
Kudos from
Kudos given to