User Activity

Hello, We are using STM32H573AII3Q in our application. One external IC is interfaced with this uC through SPI lines.  We are observing a tristate on MISO line. To investigate we isolated the uC and checked the MISO line. It is having a voltage level ...
Hello Team,We are using STM32H573AIIQ in our application. We are using SMPS to power the core supply. we have used external inductors and capacitors as per datasheet recommendations.When we tested the core supply, during power up, there is a overshoo...
Hello, We are using STM32H573AII3Q in our application. It has in-built SMPS for core power supply. Just wanted to know can we disable this SMPS and use seperate external 1V LDO to power the core?
STM32H573AII3Q is a 169 pin UFBGA SMPS package. Along with SMPS option, does it also have internal LDO for core supply? Can we use internal LDO to supply core voltage for this package?
Hello Everyone, I am using STM32H573. Do we need to connect RS232 to UART transceiver or can we directly interface Rs232 signals with UART?
Kudos given to