User Activity

Hello,I am use a winbond W25Q128JV chip which is connected to the OCTOSPI interface of my STM32H563. I read/write the flash in direct mode. The transfers are done with DMA. Everything works fine as long as the address is smaller than 0x200000 (2 MByt...
Hello,I am trying to develop an external loader application for the STM32H563ZI which is connected to a QSPI flash of type W25Q129JV. I have managed to create a project as described in the ST example. My problem is that the call to HAL_RCC_ClockConfi...
Hi there,I am working with the Nucleo-H563ZI board. The board is modified so that its hardware can act as a USB host. I am running Azure RTOS with USBx in the board. USBx is configured in host mode (not OTG) with classes HID (keyboard) and Hub. A USB...
Kudos from
Kudos given to