User Activity

Hello,I have a rather strange problem on the CM7, where code executes with half or third the speed it should.I have no idea what is causing this, but I know how to fix it: by adding one or several NOPs somewhere in the code.Example: an ISR is taking ...
I have a strange problem. I have a global uint32_t variable that counts up in the main loop and every 100 ms it gets reset in a timer-ISR. This works, but sometimes it does not.Here is the value of the variable MainCounter read out by the debugger:Th...
tl;dr: accessing external memory over debugger results in additional unwanted write accesses to adjacent memory locationsI have an FPGA that is accessed via FMC over a 16-bit async connection (16-bit data +15-bit address), sort of like an external SR...
Hello,I am trying to get the FMC to work in 16-bit synchronous mode but I only get an output with 4 clocks (64-bit) instead.In other threads [1], [2] I found that I should either switch the address from 0x60000000 to 0xC0000000 or enable the MPU, but...
Kudos given to