Hello,I am reaching out to ask if it would be possible to get some help configuring my esp01.c library.I am currently developing a library that utilizes DMA, interrupts, and a circular buffer to communicate with an ESP-01 module. The module is connec...
Hello, I would like to contact you because, following the code made on Keil uvision 5, I cannot get my interrupt to work.Objective of the code, turn on and off the LED (pb0) of the card with the button (pc13) on it itself.PCB Used : STM32F767ZI
Hello, I would like to ask you to know how it is that the PA5 pin in OUTPUT (non-pullup and non-pulldown) delivers a voltage of only 2.6 V instead of 3.3 V like the others?
Thanks in advance
Ok, I understand, but I code in bare metal with Kiel uVision5, because I would line to know how it works and I would like to reduce energy consumption.