User Activity

Hi,I am trying to write the IQ data to the SD card (i.e., write the received CTE pkt to the SD card). However, I found that Bluenrg-332ac has a cortex M0 core, which may not be able to drive an SD card. Is it possible to use this cortex M0 core for S...
Hi all,As IQ samples are used in the direction-finding feature, I am wondering how I can extract the phase information from the sampled IQ data. I tried to extract the phase by arctan(Q/I), but it changed very quickly. Is this because of the low IF a...
Hi,I am using the Bluenrg-332ac and the eval board BlueNRG-LPS STEVAL-IDB012V1.  I used the 'hci_le_connectionless_iq_report_event' function to extract IQ signals and RSSI. However, the magnitude, which is derived from the IQ samples, fluctuates dram...
Hi everyone,I am currently working on a PCB design using a Bluenrg-332ac chip. The official PCB design guideline has a resistor marked "X" as shown on the left of the figure below. But I saw the resistor soldered on the eval board. Can anyone explain...
Hi everyone,I am currently designing my own PCB board using the bluenrg-332ac chip. I want to use the ufl/SMA port to connect my antenna without connecting the PCB antenna. So I wonder how to remove the PCB antenna from the PCB layout with only UFL p...
Kudos given to