Hi, I just did the calculations with your gatt info, I have the impression that by doing the calculations as if you had a FULL_GATTDB_NVM configuration, we end up with 7 bonded devices max. (see NVM_-_FULL_GATTDB_NVM_flag )That would be consistent wi...
Hi,
The examples provided are beacons that only work in broadcast mode, i.e. sending information without connections.It is therefore not possible to connect with a p2pClient.
To do this, you need to flash a p2pClient and a p2pServer on 2 boards.Press...
Hi,In case NVM is full, only the last bonding is kept and all the previous bonding are deleted (to save space)Normally there is an hardware_error_event message before NVM is full (NVM_Warning).By the way, it is possible to get all the devices bond us...
Hi, there,BLE Audio (Auracast), is available on STM32WBA and not STM32WB.You can find the answer to your question right here:Bluetooth_LE_Audio_STM32WBA_LC3_Codec#Clock_tree_and_Low_power If you would like more information on BLE Audio, you can find ...
Hi,
I don't know your use case but if it's possible, the simplest thing would be to do the opposite, i.e. to filter the Servers on the Customer side using the ADV data.
If this is not possible, the best solution would be to use the Filter Accept List...