User Activity

Can anyone confirm that the Build Analyzer in the CubeIDE works when using the CMake toolchain? For compatibility reasons I'm currently stuck at IDE version 1.16.1. I created a fresh CMake Project for a Nucleo board (U545). It creates the elf and map...
Hi, I am using 3 DMA channels of DMA1 on a STM32G4* to transfer data from the 3 ADCs to mem. At a certain point I want to make sure that all transfers are done and enter a while loop:  uint32_t timeoutCnt = 0; while(!LL_DMA_IsActiveFlag_TC1(DMA1) || ...
Using STM32_Programmer_CLI.exe (v2.13.0, on Win10) I try to connect via ST-Link / SWD, It works perfectly in the GUI but if I trySTM32_Programmer_CLI --connect port=SWD ap=1nothing happens, not even an error, it just terminates. I can even write nons...
Kudos from