User Activity

I can build a “timer” using a counter with “decoder” circuitry to create an output signal at a specific time after starting the counter...Alternately, after each clock to the counter, the counters output value could be compared to some register value...
In the ATM32H747XI datasheet Table 9 on page 89...As I read this table... Examples are...Pin Name PA1 Alternate Function AF1 = TIM2_CH2Pin Name PA2 Alternate Function AF2 = TIM5_CH3Question 1:For PA0 AF1, there are two functions listed... TIM2_CH1/TI...
Newbie here.I discovered the STM32 Nucleo development boards and there seem to be lots of models.After clicking and clicking I can't seem to find the one for the STM32H747XI - TFBGA240+25 Package...Or at least one with the same number of pinouts... e...
Kudos given to