cancel
Showing results for 
Search instead for 
Did you mean: 

yocto - optee/export-user_ta missing files

edwardmcl
Associate II

Doing a build using yocto mickledore it fails with this error message.

CMake Error at host/xtest/CMakeLists.txt:3 (include):
include could not find requested file:
... /tmp-glibc/work/osd32mp1_brk-ostl-linux-gnueabi/optee-test/3.19.0+gitAUTOINC+ab9863cc18-r0/recipe-sysroot/usr/include/optee/export-user_ta/host_include/conf.cmake

The kernel is built correctly but it fails on building optee-test.

It seems that the directories and files in export-user_ta are not auto-generated. What bitbake configuration makes this happen?

 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Gregory PLANCHON
ST Employee

Hi,

 

Would it be possible to have the complete log and the command you use?

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
 

Hi,

 

can you tell me which command you use?

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.