User Activity

Hi, I'm using an STM32U5 DK and I'm comfortable with TouchGFX and its code generation features. However, I'm struggling to achieve the same results manually, as there are many changes in both hardware configuration and TouchGFX files. Can anyone guid...
I’ve been working on a project for a while and initially generated the code only once at the beginning to set up the hardware configuration. Recently, I updated STM32CubeIDE from version 1.14.1 to 1.15.0. After updating, I regenerated the code withou...
Hello Community,I'm currently facing an issue with entering the USART bootloader mode on my STM32U5 development kit (STM32U5A9JDK). Despite following the standard procedure, the device refuses to enter bootloader mode, and I'm hoping someone here mig...
Hello everyone,I'm currently working with a custom board that utilizes the STM32U599 microcontroller, and I'm attempting to establish communication with an SD card. The IDE I'm using presents the option of FileX alongside ThreadX; however, my applica...
 Hello Community,I'm currently facing a challenging issue in my project that involves the TouchGFX framework on an STM32u59dk board, specifically related to the LTDC interrupt mechanism and its integration with the TouchGFX HAL.Despite having the LTD...
Kudos given to