User Activity

Hello,I've updated my STM32CubeIDE to the latest version (1.13.1) and verified that some annoying bugs are still there. I'm curious is there a dedicated place where to report them?I'm talking about really a basic functionality which should be working...
Hello,I've reported my problem with ST-Link GDB server here:https://community.st.com/s/question/0D53W00002BBBlsSAH/stm32cubeide-debugging-issues-of-code-placed-in-sram-stm32h7-mcubut thread evolves and it more and more look like a real bug in ST-Link...
Hello,I'm using latest STM32CubeIDE (1.12.0) on Linux Ubuntu 20.04 and on Apple Ventura macOS on M1 mini. I'm using also stm32h757i-eval board for this testing. I'm using RTOS (RTEMS) code for testing, but IMHO it's not a problem of RTOS/RTEMS here....
Hello,I'm curious if there is any way how to load correctly linked elf file into the SDRAM of st32h757i-eval board. By correctly linked elf I mean everything is either linked into SDRAM or to some of the SRAMs. E.g. readelf -S of the elf looks:There ...
Hello,I have stm32h757i-eval board here. I've used stm32cubeprogrammer to edit OB where I've unselected M7 core from booting and left just M4 selected. This was done in intention to boot just M4 core and leave M7 core halted.When I modified OB this w...
Kudos from