HI all, I am Ragu, and I need to flash SPC560b50l5 chip using SPC560b54l5 discovery board. I use PLS adapter setting in document as they mentioned but it not works?. Below I attached JTAG connection circuit diagram which I use. I probe the ...
Hi all, At-least I found one way to do configure GPIOs mode(input or output) at run time. I found that static const spc_siu_init_t spc_siu_init[] structure present in board.c file contains all our pins configuration but it is a constant structure; so...