cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO32X driver

DGiov.1
Associate III

Hello,

I'm looking for the drivers for the LSM6DSO32X. In the example code I found the drivers for LSM6DSO32 and for LSM6DSOX which are similar but not identical. Are them available somewhere?

Davide

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TSand.1
Associate III
5 REPLIES 5
TSand.1
Associate III

Hi, there are C drivers for this part on Github, check there!

https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm6dso32x_STdC

DGiov.1
Associate III

Hi, thank you.

I was looking in the wrong place (STM32CubeExpansion_MEMS1_V8.3.0).

DGiov.1
Associate III

Wait, that repository contains only the register definitions with part of the funtions (lsm6dso32x_reg.c/.h files).

I expected also the lsm6dso32x.c/.h, such as for the other sensors in STM32CubeExpansion_MEMS1_V8.3.0\Drivers\BSP\Components. Are them available?

TSand.1
Associate III

you can insert the github drivers in the STM32 project accounting for the specific hardware pinout, or just use the lsm6dsox drivers, the only difference with lsm6dso32x is in the increase full scale up to 32g. Hope this help.

DGiov.1
Associate III

That actually was my second option. Thank you.