User Activity

I'm trying to configure the ADC to read to values at a specific time in my system that uses the STM32G474.I have two channels of peak current mode control using the HRTIMER. The outputs are reset from either a comparator event or max duty cycle compa...
I have an STM32G474 project that has been working for some time but the latest update doesn't generate code from the .ioc config GUI.If I make I make changes in the editor and select generate code, the pop flashes quickly and goes away but no code ge...
I generated code using ToughGFX 4.13.0 for the STM32F769I_DISCO board. I was able to run target in ToughGFX and import the code into the CubeIDE. There were missing files that needed to be deleted from the project to get it to build.But after that, I...