cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I change sampling frequecy of acc sensors in en.fp-sns-allmems2_v2.1.0?

NMart.1
Associate III

I'm using STEVAL-MKSBOX1V1 for vibration analysis and I want to change sampling frecuency. I did it in the past with other versions of the project but now it has chan a little. I changed the ODR in the file lsm6dsox.c , but I also need to change the frequency in which the parameter is update. In other projects, this parameter was in the file Target_features.h (shown in image 1)Now in this file these parameters don't exist. I found this ones on other file,

ALLMEMS2_config.h (shown in image2), but he one related with inertial sensors is missing. Where can I found it?

Thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Salvatore Curti
ST Employee

Sorry for very late aswer.

I suppose you have find the soluction but belowe you can find my aswer.

If you refer at the Acc/Gyro/Mag values, you can find this parameter in the file main.c.

The mane of the parameter is: DEFAULT_uhCCR4_Val

Regards.